EIO0000003527.05

Parts Identification (HMIST6200)

Front

Top

Bottom

Rear

A: Status LED

B: Battery slot

C: Hook

D: Ethernet interface (ETH1)

E: Serial interface (RJ-45, RS-232C/485) (COM1)

F: Power plug connector

G: Safety alert symbol*1

H: USB (Type A) interface

I: USB (micro-B) interface

*1 Identifies the safety messages about the battery in Replacing the Battery

WARNING
UNINTENDED EQUIPMENT OPERATION
  • Do not connect the product to the computer with the USB (micro-B) cable unless the product is powered by the power cable.
  • Remove the USB (micro-B) cable before communicating with the host controller and other types of equipment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?