EIO0000003527.05

Package Contents

Verify all items listed here are present in your package.
Please contact customer support immediately if you find anything damaged or missing.

WARNING
UNINTENDED EQUIPMENT OPERATION
Do not use damaged products or accessories.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

1 HMIST6•00 x 1

2 Installation gasket (attached to this product) x 1

3 DC power supply connector x 1

4-1 Installation fasteners for HMIST6200 x 2

4-2 Installation fasteners for HMIST64/65/6600 x 4, HMIST6700 x 6

5 Quick reference guide x 1

Product Revision and QR Code

You can identify the product version (PV), revision level (RL), and the software version (SV) from the product label.

NOTE: Depending on the model, the product label may not be marked RL.

You can also check the contents of this manual by using the QR code on the product label. Confirm the location of the QR code below and refer to the manual.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?