Installation Procedure (HMIST6200)
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
Installing Using Installation Fasteners
|
Step |
Action |
|---|---|
|
1 |
Place this product on a clean and level surface with the screen facing down. |
|
2 |
Check that this product's gasket is seated securely into the bezel's groove, which runs around the perimeter of the display panel frame. NOTE: Always
use the installation gasket, since it absorbs vibration in addition
to repelling water. For the procedure on replacing the installation
gasket, refer to Replacing the Installation Gasket.
|
|
3 |
Based on this product's Panel Cut Dimensions, open a mount-hole on the panel and attach this product to the panel from the front side. NOTE: This product has a hook at the top to prevent it from
falling. Insert the bottom part of the product into the panel opening,
and then insert the top part while pushing the hook down.
1 Hook |
|
4 |
Insert the installation fastener hooks into the insertion slots of this product. 1 Insertion slots 2 Installation fastener |
|
5 |
In a clockwise direction, tighten the installation fastener's screws with a screwdriver. The necessary torque is 0.5 N•m (4.4 lb-in). 1 Installation panel |
| NOTICE |
|---|
|
BROKEN ENCLOSURE
Do not exert more torque than the amount specified.
Failure to follow these instructions can result in equipment damage.
|
Installing Using Spring Clips
CAUTION |
|---|
|
SPRING LOADED MECHANISM
Do not release the spring clip mechanism near your face.
Failure to follow these instructions can result in injury or equipment damage.
|
|
Step |
Action |
|---|---|
|
1 |
Place this product on a clean and level surface with the screen facing down. |
|
2 |
Check that this product's gasket is seated securely into the bezel's groove, which runs around the perimeter of the display frame. NOTE: Always use the
installation gasket, since it absorbs vibration in addition to repelling
water. For the procedure on replacing the installation gasket, refer
to Replacing the Installation Gasket.
|
|
3 |
Based on this product's Panel Cut Dimensions, open a mount hole on the panel and attach this product to the panel from the front side. NOTE: This product has a hook at the top to prevent it from
falling. Insert the bottom part of the product into the panel opening,
and then insert the top part while pushing the hook down.
1 Hook |
|
4 |
Press the spring clip hooks into the insertion slots on this product. Adjust the spring clips for the panel thickness by turning it over:
Side of the spring clip 1 Hook for position 1 2 Hook for position 2 3 Insertion slots |
|
5 |
Lock the spring clips by simultaneously pressing the top and bottom of the clip. 1 Installation panel 2 Spring clip |
|
6 |
To remove the spring clips, unlock the clips by pressing on the back of the clip until you hear a click. |
CAUTION |
|---|
|
RISK OF INJURY
Do not drop this product when you remove it from the panel.
Failure to follow these instructions can result in injury or equipment damage.
|
DANGER


CAUTION