EIO0000003527.05

Accessories

Products may change or be discontinued without notice. Please check our website for the latest information.
www.se.com/docs

For host controllers and connection cables, refer to the corresponding device driver manual of your screen editing software.

Product name

Product number

Description

Serial interface

RJ-45 to D-Sub 25 pin Conversion Cable

XBTZG939

Connects a D-Sub 25-pin cable to this product (RJ-45).

9-pin to 25-pin RS-232C Conversion Cable

XBTZG919

Connects a standard RS-232C cable (D-Sub 25-pin socket) to this product (D-Sub 9-pin plug).

COM Port Conversion Adapter

XBTZGCOM1

Connects optional RS-422 communication items to serial interface (RS-232C).

RS-232C Isolation Unit

XBTZGI232

Connects a host controller to this product and provides isolation
(RS-232C and RS-422 are switchable).

RS-485 Isolation Unit

XBTZGI485

Connects a host controller to this product with isolation.

USB (micro-B) interface

USB Transfer Cable

HMIZG936

Cable for transferring screen data from a PC (USB Type A) to this product (USB micro-B).

USB (micro-B) Front Cable

HMIZSUSBB2

Extension cable that attaches USB interface to front panel.

USB (Type A) interface

USB Front Cable

XBTZGUSB

Extension cable that attaches USB interface to front panel.

USB Clamp Type A (1 port)

HMIZGCLP1

Clamp to prevent disconnection of USB cable (USB Type A, 1 port, 5 clamps/set).

Others

Screen Protection Sheet

HMIZD66W

Disposable, dirt-resistant sheet for 12-inch Wide screen (5 sheets/set).

UV Protection Sheet

HMIZUV6W

Sheet to protect the display from dirt and ultraviolet light, for 12-inch Wide screen (1 sheet).

Screen Protection Sheet with UV Protection

HMIZG60W

Disposable, dirt-resistant and ultraviolet protection sheet for 4-inch Wide screen (1 sheet/set).

HMIZG63W

Disposable, dirt-resistant and ultraviolet protection sheet for 7-inch Wide screen (1 sheet/set).

HMIZG65W1

Disposable, dirt-resistant and ultraviolet protection sheet for 10-inch Wide screen (1 sheet/set).

HMIZG67W

Disposable, dirt-resistant and ultraviolet protection sheet for 15-inch Wide screen (1 sheet/set).

Spring Clip

XBTZ3002

Fasteners to attach this product to the mounting surface for HMIST6200.

Maintenance Accessories

Product name

Product number

Supported product

Description

Installation fastener

HMIZSFIX2

HMIST6200

Installation fastener (2 pieces/set).

HMIZSFIXTF1

HMIST6400, HMIST6500, HMIST6600, HMIST6700

Installation fastener (2 pieces/set).

Installation gasket

HMIZS51W1

HMIST6200

Provides dust and moisture resistance when this product is installed into a solid panel (1 piece).

HMIZS53W1

HMIST6400

HMIZS55W1

HMIST6500

HMIZS56W1

HMIST6600

HMIZS57W1

HMIST6700

DC power supply connector

XBTZGPWS1

All

Connector to connect DC power supply cables.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?