Installation Procedure (HMIST64/65/66/6700)
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
Installing Using Installation Fasteners
|
Step |
Action |
|---|---|
|
1 |
Place this product on a clean and level surface with the screen facing down. |
|
2 |
Check that this product's gasket is seated securely into the bezel's groove, which runs around the perimeter of the display panel frame. NOTE: Always
use the installation gasket, since it absorbs vibration in addition
to repelling water. For the procedure on replacing the installation
gasket, refer to Replacing the Installation Gasket.
|
|
3 |
Based on this product's Panel Cut Dimensions, open a mount-hole on the panel and attach this product to the panel from the front side. NOTE: This product has a hook at the top to prevent it from
falling. Insert the bottom part of the product into the panel opening,
and then insert the top part while pushing the hook down.
1 Hook |
|
4 |
Insert the installation fastener hooks into the insertion slots of this product. 1 Insertion slots 2 Insertion slots (HMIST6700 only) 3 Installation fastener 4 Installation panel |
|
5 |
In a clockwise direction, tighten the installation fastener's screws with a screwdriver. The necessary torque is 0.5 N•m (4.4 lb-in). NOTE: The
installation fasteners can be screwed by hand too.
|
| NOTICE |
|---|
|
BROKEN ENCLOSURE
Do not exert more torque than the amount specified.
Failure to follow these instructions can result in equipment damage.
|
DANGER