Certifications and Standards
The certifications
and standards listed below may include those that are not yet acquired.
Please check the product marking and the following URL for the latest
acquisition status.
www.se.com/ww/en/download
Agency Certifications
-
Underwriters Laboratories LLC., UL 61010-2-201 and CSA C22.2 No.61010-2-201, Industrial Control Equipment
-
EAC certification (Russia, Belarus, Kazakhstan)
Compliance Standards
Europe:
CE/UKCA
-
Directive 2014/30/EU (EMC)
Australia, New Zealand:
-
RCM
Korea:
-
KC
Hazardous Substances
This product is designed to be compliant with the following environmental regulations, even if the product may not fall directly in the scope of the regulation:
-
RoHS, Directive 2011/65/EU and 2015/863/EU
-
RoHS China, Standard GB/T 26572
-
REACH regulation EC 1907/2006
End of Life (WEEE)
The product contains electronic boards. It must be disposed of in specific treatment channels. The product contains cells and/or storage batteries which must be collected and processed separately when they have run out and at the end of product life (Directive 2012/19/EU).
Refer to Maintenance when extracting cells and batteries from the product. These batteries do not contain a weight percentage of heavy metals over the threshold notified by European Battery Regulation 2023/1542.