EIO0000003527.05

Precautions for Building into an End-use Product

This product is designed for use on flat surfaces of IP65F, UL 50/50E, Type 1, Type 4X (indoor use only) and Type 13 enclosures.

Be aware of the following when building this product into an end-use product:

  • The rear face of this product is not approved as an enclosure. When building this product into an end-use product, be sure to use an enclosure that satisfies standards as the end-use product's overall enclosure.

  • Install this product in an enclosure with mechanical rigidity.

  • This product is not designed for outdoor use. UL certification obtained is for indoor use only.

  • Install and operate this product with its front panel facing outward.

NOTE:
  • The necessary torque is 0.5 N•m (4.4 lb-in).

  • IP65F is not part of the UL certification.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?