7EN02-0438-14

Resetting accumulated energy using the display

  1. Navigate to the Partial Active E or Partial Reactive E screen. The screen displays the date of the last reset. For example:
     

    A

    Date of last reset

         
  2. Press and hold . The Reset screen appears.
  3. Press to confirm the reset and enter the meter password when prompted.
    NOTE: Regardless of the screen you use to access this reset, accumulations of both Partial Active Energy and the Partial Reactive Energy (if available) are cleared.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?