7EN02-0438-14

Resetting peak demand using the display

  1. Navigate to any of the below listed screens:
    • I1 Demand Peak

    • I2 Demand Peak

    • I3 Demand Peak

    • P Demand Peak

    • Q Demand Peak

    • S Demand Peak

     

    A

    Date and time of peak demand

         
  2. Press and hold . The Reset screen appears.
  3. Press to confirm the reset and enter the meter password.
    NOTE: Once the peak demand is reset, the date and time are not displayed till the next peak demand is captured.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?