DOCA0142EN-11

Device Identification

Device Name Configuration Procedure

Step

Action

Result

1

From the IFE menu bar, click Diagnostics.

Opens the Diagnostics page.

2

From the Diagnostics menu, in the Product Information submenu, click Device Identification.

Opens the Device Identification page.

List of Parameters in Device Identification

Parameter

Description

Device name

Device name which is updated in the device name field

Product name

Name of the product

Serial number

Device serial number

Product model number

Device model number

Firmware version

Current firmware version

Unique Identifier

Combination of MAC address and the time

MAC address

Unique MAC address

IPv4 address

IP address of the IFE interface

IPv6 link local address

Address used to communicate on the local network

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?