Email Service
Description
The page allows you to activate email service and to set the Simple Mail Transfer Protocol (SMTP) server settings. The SMTP is a set of communication guidelines that allow the software to transmit an electronic mail over the Internet. It is a program used for sending messages to other computer users based on email addresses.
The users with Installer or Engineer roles can change the email service settings.
Navigation to the Email Service Page
To view the page, click .
Email Service
|
Parameter |
Description |
|---|---|
|
|
Enables the Email service (disabled by default). |
Email SMTP Server Settings
|
Parameter |
Description |
Value |
|---|---|---|
|
|
Allows you to enter an email server address (SMTP server). NOTE: Contact your network administrator to know the IP address or the
name of the SMTP server.
|
– |
|
|
Allows you to select the connection security mode. |
|
|
|
Allows you to enter the SMTP server port. |
|
|
|
Allows you to enable Authentication if the SMTP server requires login information (disabled by default). |
- |
|
|
Allows you to enter the SMTP account login name. |
– |
|
|
Allows you to enter the SMTP account password. |
– |
Email Sender Address Settings
|
Parameter |
Description |
|---|---|
|
|
Allows you to enter the email address of the administrator. |
The can be used in different ways:
-
Use the as a context provider: If you do not want to receive any reply, and only notify the recipient, use as contextual information. The syntax includes “no-reply”, “device name”, “site name”, @a validated domain.com, .net, and so on.
-
Create an alias in the to allow replies to be sent to the person in charge of an alarm: An email can be sent to multiple people who are responsible for a specific appliance. This feature allows the receivers to reply to follow up with the responsible person.
For example, the facility manager would receive an email from an alarm. Facility manager can send a reply email to the maintenance contractor to follow up on the action.
Email Language Settings
|
Parameter |
Description |
Setting |
|---|---|---|
|
|
Allows you to select the language of the email body. |
|
Email Test Settings
|
Parameter |
Description |
|---|---|
|
|
Allows you to enter the email address of the recipient to test the delivery of the email. |
The feature enables connection from the IFE interface to the service.
Click to send the test email to the recipient address for test. If the test emails are not received, the Internet connection needs to enable the email ports (port 25 or 465 or 587). The required setting of the port is done in accordance between the IFE interface that sends the email and the site router settings.