DOCA0142EN-12

Syslog Service

Description

The SYSLOG SERVICE page allows you to configure the Syslog server settings for the security logs generated by the IFE interface.

The IFE interface logs 2048 security events before the oldest events are over written by newer events.

Ensure the security logs are exported on a regular basis from the IFE interface by:

  • Manual log export in CSV format.

  • Automatic export of the security logs using the Export Interval parameter.

NOTE: Syslog server can also be configured using the EcoStruxure Cybersecurity Admin Expert software. For more information, refer to CAE_UM_EN EcoStruxure Cybersecurity Admin Expert Guide.

Ensure that the Syslog server is installed in your monitoring PC.

Navigation to the Syslog Service Page

To view the SYSLOG SERVICE page, click SECURITY > SYSLOG SERVICE.

Syslog Service Parameters

Parameter

Description

Value

Syslog Logging Service

Allows you to enable or disable the Syslog service.

Default setting: Disabled

SysLog Server Address

Allows you to enter the server name or IP address of the Syslog server.

Connection Mode

Allows you to select the connection type.

Default setting: TCP

SysLog Server Port

Allows you to enter the Syslog server port number.

Setting range:1–65534

Default setting: 801

Export Interval

Allows you to set the interval for the export of Syslog logging file.

Setting range:10–3600 s

Default setting: 300 s

Export to CSV

Click Export to CSV to export the security log files in CSV format. The content of the security logs comply with the Syslog standard.

Test Connection

Click Test Connection to verify the connection between the IFE interface and Syslog server. During the test, the IFE interface will connect with the Syslog server and the user will be notified if the connection is established or not.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.