DOCA0142EN-12

Schematics with MasterPacT NT/NW, ComPacT NS, PowerPacT P- and R-frame Circuit Breakers

Description

Depending on the type of circuit breaker used, connect the IFE interface to the circuit breaker using one of the following configurations:

  • Connection of the IFE interface to a fixed manually-operated circuit breaker with a BCM ULP module:

    • ComPacT NS 630b-3200 circuit beakers

    • PowerPacT P- and R-frame circuit breakers

  • Connection of the IFE interface to a fixed electrically-operated circuit breaker with a BCM ULP module:

    • MasterPacT NT/NW circuit beakers

    • ComPacT NS 630b-1600 circuit beakers

    • PowerPacT P-frame circuit breakers

  • Connection of the IFE interface to a drawout circuit breaker with a BCM ULP module and its respective IO module:

    • MasterPacT NT/NW circuit beakers

    • ComPacT NS 630b-1600 circuit beakers

    • PowerPacT P-frame circuit breakers

For more information, refer to DOCA0093•• ULP (Universal Logic Plug) System - User Guide.

ULP Connection

NOTICE
HAZARD OF EQUIPMENT DAMAGE
  • Never connect an Ethernet device to a RJ45 ULP port.
  • The RJ45 ULP ports of IFE interface are for ULP modules only.
  • Any other use can damage the IFE interface or the device connected to the IFE interface.
  • To check if a ULP module is compatible with the RJ45 ULP ports of IFE interface, refer to DOCA0093•• ULP (Universal Logic Plug) System - User Guide.
Failure to follow these instructions can result in equipment damage.

All connection configurations require the BCM ULP cord.

When the second RJ45 ULP port is not used, it must be closed with a ULP line termination.

A

Circuit breaker BCM ULP cord or RJ45 plug/plug ULP cord

B

ULP line termination

Connection of the IFE Interface to a Fixed Manually-Operated Circuit Breakers

Applicable for:

  • ComPacT NS 630b-3200 circuit beakers

  • PowerPacT P- and R-frame circuit breakers

A

IFE Ethernet interface for one circuit breaker

B

ULP line termination

C

Circuit breaker BCM ULP cord

D

BCM ULP circuit breaker communication module

E

Fixed manually-operated circuit breaker

Connection of the IFE Interface to a Fixed Electrically-Operated Circuit Breakers

Applicable for:

  • MasterPacT NT/NW circuit beakers

  • ComPacT NS 630b-1600 circuit beakers

  • PowerPacT P-frame circuit breakers

A

IFE Ethernet interface for one circuit breaker

B

ULP line termination

C

Circuit breaker BCM ULP cord

D

Fixed terminal block

E

BCM ULP circuit breaker communication module

F

Fixed electrically-operated circuit breaker

Connection of the IFE Interface to the Drawout Circuit Breakers

Applicable for:

  • MasterPacT NT/NW circuit beakers

  • ComPacT NS 630b-1600 circuit beakers

  • PowerPacT P-frame circuit breakers

A

IFE Ethernet interface for one circuit breaker

B

ULP line termination

C

RJ45 plug/plug ULP cord

D

Circuit breaker BCM ULP cord

E

Circuit breaker disconnected position contact (CD)

F

Circuit breaker cradle

G

BCM ULP circuit breaker communication module

H

Drawout circuit breaker

I

Drawout terminal block

J

Circuit breaker connected position contact (CE)

K

Circuit breaker test position contact (CT)

L

IO input/output application module for one circuit breaker

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.