DOCA0142EN-11

Schematics with ComPacT NSX Circuit Breakers

General Description

Depending on the configuration of the ComPacT NSX circuit breaker, connect the IFE interface to the circuit breaker using one of the following configurations:

  • Connection of the IFE interface to the MicroLogic trip unit

  • Connection of the IFE interface to the BSCM or BSCM Modbus SL/ULP module

  • Connection of the IFE interface to the BSCM or BSCM Modbus SL/ULP module and to the MicroLogic trip unit

For more information, refer to DOCA0093•• ULP (Universal Logic Plug) System - User Guide.

ULP Connection

WARNING
HAZARD OF ELECTRIC SHOCK
For system voltage greater than 480 Vac:
  • Use the insulated NSX cord LV434204.
  • Do not use NSX cords LV434200, LV434201, and LV434202.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTICE
HAZARD OF EQUIPMENT DAMAGE
  • Never connect an Ethernet device to a RJ45 ULP port.
  • The RJ45 ULP ports of IFE interface are for ULP modules only.
  • Any other use can damage the IFE interface or the device connected to the IFE interface.
  • To check if a ULP module is compatible with the RJ45 ULP ports of IFE interface, refer to DOCA0093•• ULP (Universal Logic Plug) System - User Guide.
Failure to follow these instructions can result in equipment damage.

All connection configurations require the NSX cord. The insulated NSX cord is mandatory for system voltages greater than 480 Vac.

A

NSX cord or RJ45 plug/plug ULP cord

B

ULP line termination

Connection of IFE Interface to MicroLogic Trip Unit

A

IFE Ethernet interface for one circuit breaker

B

ULP line termination

C

NSX cord

D

MicroLogic trip unit

Connection of IFE Interface to BSCM or BSCM Modbus SL/ULP Module

A

BSCM or BSCM Modbus SL/ULP module

B

NSX cord

C

ULP line termination

D

IFE Ethernet interface for one circuit breaker

Connection of IFE Interface to BSCM or BSCM Modbus SL/ULP Module and to MicroLogic Trip Unit

A

BSCM or BSCM Modbus SL/ULP module

B

MicroLogic trip unit

C

NSX cord

D

ULP line termination

E

IFE Ethernet interface for one circuit breaker

Connection of IFE Interface to a Circuit Breaker for System Voltage Greater than 480 Vac

A

IFE Ethernet interface for one circuit breaker

B

ULP line termination

C

RJ45 plug/plug ULP cord

D

Insulated ULP module for system voltage greater than 480 Vac

E

Insulated ULP cord for system voltage greater than 480 Vac

F

Connector for ComPacT NSXcircuit breaker internal connection

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.