DOCA0142EN-12

Set Device Time

Description

The Set Device Time page allows you to synchronize the date and time of the circuit breaker connected to the IFE interface to IFE interface date and time. The time is set automatically. This page is used to get the circuit breaker time.

List of Parameters in Set Device Time

Parameter

Description

Device Selection

Allows you to select the circuit breaker that is to be synchronized with IFE interface date and time.

Localized Time

Displays the time of the circuit breaker.

Status

Displays the status of the circuit breaker.

Get Time

Allows you to get the time of the circuit breaker.

Set Device Time

Not applicable.

Setting the Device Time

Step

Action

Table

1

From the IFE menu bar, click Control.

Opens the Control menu.

2

From the Control menu, click Set Device Time.

Opens the Set Device Time page.

3

Select the circuit breaker from the Set Device Time page and then click Get Time.

The date and time of the circuit breaker gets synchronized with the IFE interface date and time, and the status is updated as successful.

NOTE: If the circuit breaker fails to synchronize with IFE interface date and time, then the status is updated as unsuccessful.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.