Schematics with MasterPacT MTZ Circuit Breakers
Description
The IFE interface is connected to the MasterPacT MTZ circuit breaker through its ULP port module.
For more information, refer to the ULP System User Guides in Related Documents.
ULP Connection
NOTICE |
---|
HAZARD OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
All the connection configurations require the RJ45 plug/plug ULP cord.
Connection of the IFE Interface to a MasterPacT MTZ Circuit Breaker
Connect the IFE interface to the ULP port module on a MasterPacT MTZ circuit breaker by using the ULP cord.

A |
IFE Ethernet interface for one circuit breaker |
B |
ULP line termination |
C |
RJ45 plug/plug ULP cord |
D |
ULP port module |
E |
MasterPacT MTZ fixed circuit breaker |