DOCA0142EN-07

SNMP

Description

The SNMP page displays the diagnostic data of SNMPV1 Agent parameters.

The users with Installer or Engineer roles can consult the Diagnostics pages.

Navigation to the SNMP Page

To view the SNMP page, click DIAGNOSTICS > COMMUNICATION > SNMP .

SNMPV1 Agent Parameters

Parameter

Description

State

Displays the state of SNMPV1 agent.

Received Packets

Number of packets received from the network.

Emitted Packets

Number of packets transmitted from the network.

Emitted Traps

Number of traps transmitted on detection of a change as asynchronous notification from agent to manager.

Received Bad Community Names

Number of received bad community names.

Emitted Bad Community Names

Number of transmitted bad community names.

Click Reset Counters to reset the statistics values to 0.

If the IFE interface is switched off or if it is reset due to a configuration change or another event, the statistics values are reset to 0.

QR code for this page

Was this helpful?