7EN02-0407-04

Display interface

Use the device display to perform various tasks such as configuring the device, displaying status screens, acknowledging alarms, or viewing events.

1 Screen identification area containing a menu icon, and the name of the menu or the parameter
2 Information area displaying information specific to the screen (measurement, insulation alarm, settings)
3 Navigation buttons

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?