7EN02-0407-04

Accessories

Accessories are required depending on the type of installation on which the device is installed.

Accessories list

Accessory Catalog number
Toroid Refer Vigilohm catalog

Toroids

The toroids are used to connect the device to the channels of the system, which can be monitored. The compatible toroids are:

  • TA30

    NOTE: This toroid is advised for IFL12H.

  • PA50

  • IA80

  • MA120

  • SA200

  • GA300

  • TOA80

  • TOA120

Refer to the Vigilohm catalog for the most up to date listing of compatible devices. Refer to the toroid user guide for specifications.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?