7EN02-0407-04

Channel Name

You can set the channel name of your preference for all 12 channels.

The channel name can be set only in English. The allowed characters are:

  • A to Z

  • a to z

  • 0 to 9

  • Special characters (Hyphen-minus (-), Slash (/), Percent(%), Full stop (.), (blank))

The length of the channel name is automatically adjusted depending on the character selection. For example, if the channel name contains only the character “W”, then the maximum length is 8 characters and if the channel name contains only the character “I”, then the maximum length is 18 characters.

Use the following contextual buttons for editing:

  • to modify the selected character.

  • to select the character to the right of the one that is currently selected, or to loop back to the character on the left.

  • to confirm the channel name.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?