Alarm event records
-
A "primary" record, which is created when the insulation alarm occurs. This contains the insulation value.
-
A "secondary" record, which is created for the following type of events:
-
Acknowledged insulation alarm
-
Power failure or power cycle
-
Toroid disconnect
-
Locating signal unavailable
-
Product or channel error
-
Automatic commission initiation
-
Description of an Event Record in the Log
Register | Unit | Type | Range | Description |
---|---|---|---|---|
Word 1 | – | Uint16 | 1...65535 | Event record number |
Word 2 Word 3 Word 4 Word 5 |
– | Uint64 | – | Time tagging of event (using the same code as for the product date/time) |
Word 6 Word 7 |
– | Uint32 |
|
Record identifier:
|
Word 8 Word 9 Word 10 Word 11 |
– | Uint64 | – |
Depending on the type of record (primary or secondary):
|
Word 12 | – | Uint16 | 1...65534 |
Primary/secondary record identifier for the event:
|
Example of an event
The next 2 records relate to an example insulation alarm that occurred on October 1, 2010 at 12:00 pm and was acknowledged at 12:29 pm.
Record number: 1
Address | Register | Unit | Type | Value | Description | ||
---|---|---|---|---|---|---|---|
dec | hex | dec | hex | ||||
20002 | 4E22 | 20003 | 4E23 | – | Uint16 | 1 | Record number |
20003 | 4E23 | 20004 | 4E24 | – | Uint64 |
|
Date when insulation alarm occurred (October 1, 2010, 12:00 pm) |
20007 | 4E27 | 20008 | 4E28 | – | Uint32 |
|
Record identifier:
|
20009 | 4E29 | 20010 | 4E2A | Ohm | Uint64 | 10000 | Insulation resistance value at the time of the insulation alarm |
20013 | 4E2D | 20014 | 4E2E | – | Uint16 | 1 | Secondary record identifier for the event |
Record number: 2
Address | Register | Unit | Type | Value | Description | ||
---|---|---|---|---|---|---|---|
dec | hex | dec | hex | ||||
20014 | 4E2E | 20015 | 4E2F | – | Uint16 | 2 | Record number |
20015 | 4E2F | 20016 | 4E30 | – | Uint64 |
|
Date when insulation alarm acknowledged (October 1, 2010, 12:29 pm) |
20019 | 4E33 | 20020 | 4E34 | – | Uint32 |
|
Record identifier:
|
20021 | 4E35 | 20022 | 4E36 | – | Uint64 | 8 | Value of insulation alarm register at the time of insulation alarm acknowledgement |
20025 | 4E39 | 20026 | 4E3A | – | Uint16 | 2 | Secondary record identifier for the event |