7EN02-0407-04

Reset

You can reset logs. Further, you can perform factory reset.

You can access the device reset parameters by selecting Menu > Settings > Reset.

The reset parameters are Reset Logs and Factory Reset.

On performing reset of logs, the existing logs information is erased but the settings parameter value remains unchanged. On performing factory reset, the device restarts and automatic commissioning is initiated. Also, settings parameter values are reset to default.

The complete list of settings parameters, its default value, and allowed values are:

The following table is profiled. Check for row profiling before making any content change.
Parameter Default Value Allowed Values
Ins. Alarm

50 kΩ

50...200 kΩ

Channel Name CHANNEL – 1 to CHANNEL – 12 for 12 channels
  • A to Z

  • a to z

  • 0 to 9

  • Special characters (Hyphen-minus (-), Slash (/), Percent(%), Full stop (.), (blank))

The length of the channel name is automatically adjusted depending on the character selection. For example, if the channel name contains only the character “W”, then the maximum length is 8 characters and if the channel name contains only the character “I”, then the maximum length is 18 characters.

Ins. Al. Relay FS
  • FS

  • Std.

Address 1 1...247
Baudrate 19200
  • 4800

  • 9600

  • 19200

  • 38400

Parity Even
  • None

  • Even

  • Odd

Modify Password 0000 0000...9999
Activation (Password) OFF
  • ON

  • OFF

Contrast 50% 10...100%
Backlight 100% 10...100%

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.