7EN02-0407-04

Insulation measurements

The device monitors the insulation per connected channel of ungrounded power system.

The device measures and displays the insulation resistance R (Ω) continuously for 12 channels.

To view these values, navigate to Menu > Monitoring. To view each channel measurements, use the contextual menu buttons.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?