7EN02-0407-04

Insulation fault log display screen

You can the view the details of an insulation fault event by navigating to Menu > Logging.

The below table rows are profiled. Check row profiling before making any changes
1 Insulation fault value recorded
2 Type of fault recorded:

Insulation fault

NOTE: Only insulation fault is recorded as primary record.

3 Date and time when the fault appeared
NOTE: This information is stored as primary record.
4

Date and time when the fault disappeared due to any one of the following event:

  • Insulation fault acknowledgement

  • Power failure while on active alarm.

  • Toroid disconnect while on active alarm.

  • Voltage signal unavailable while on active alarm.

  • Product or channel error while on active alarm.

  • Automatic commissioning initiated while on active alarm.

NOTE: This information is stored as secondary record.

5 Number of the event displayed
6 Total number of events recorded
7 Name of the channel, where the log is recorded
8 Number of the channel, where the log is recorded
9 Up and down arrows: Use to view recorded events

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?