7EN02-0407-04

Alarm configuration

You can configure the insulation alarm threshold to suit to the electrical applications you want to monitor.

You can access the device alarm parameters by selecting Menu > Settings > Ins.Alarm.

The alarm parameter is Ins. Alarm.

You can set the parameter values for all commissioned or uncommissioned channels

To modify the parameter value, see Parameter modification using the display.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?