7EN02-0407-04

Hardware overview

Vigilohm IFL12H feature 5 terminal blocks.
A Alarm relay
B Auxiliary power supply
C Product status LED
D Communication LED
E Menu button
F No alarm LED
G Esc button
H Alarm LED
I 3 contextual menu buttons
J

Label

NOTE: Scan the QR code to view the device documentation: QR code link

K RS-485 communication
L 12 toroid connections
M Voltage input
N LCD screen
O Gasket
P Commercial reference and manufacturing data
Q

Specification Label

NOTE: Scan the QR code to view the device documentation: QR code link

R DIN mounting clip

Device commercial reference

Model Commercial reference
IFL12H IMDIFL12H
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?