7EN02-0407-04

Navigation buttons and icons

Use the display buttons to navigate through menus and perform actions.
Legend Button Icon Description
1 Menu Display the level 1 menu (Menu).
2 Esc Go back to the previous level.
3 Contextual menu button 3 Scroll up the display or move to the previous item in a list.
Access the date and time setting. If the clock icon flashes, it means that the Date/Time parameter needs to be set.

Increase a numerical value.

Modify the selected character

Select all channels to set same value of insulation alarm threshold.

Select all channels to perform manual commission.

Select each channel to set value of insulation alarm threshold.

Select each channel to perform manual commission.

4 Contextual menu button 2 Scroll down the display or move to the next item in a list.
Move one digit to the left within a numerical value. If the digit on the far left is already selected, pressing the button loops you back to the digit on the right.

Move from one character to the right of the one that is currently selected, or to loop back to the character on the left.

Move from one channel to another channel to set value of insulation alarm threshold and to select channel for manual commissioning.
5 Contextual menu button 1

Validate the selected item.

Run the auto-test manually.
Go to a menu or submenu, or edit a parameter.
Acknowledge the insulation alarm.

Exit automatic commissioning mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?