7EN02-0407-04

Password

You can set a password to limit access to configuration of the device parameters to authorized personnel only.

When a password is set, the information displayed on the device can be viewed but the parameter values cannot be edited. By default, the password protection is not activated. The default password is 0000. You can set a 4-digit password from 0000 to 9999.

To activate the password, navigate to Menu > Settings > Password > Activation and select ON.

To modify the password, navigate to Menu > Settings > Password > Modify Password and edit the new password. To modify the parameter value, see Parameter modification using the display.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?