7EN02-0407-04

Information icons

Icons in the information area of the LCD display provide information such as what menu is selected and the insulation alarm status.

The following table is profiled. Check for row profiling before updating any content
Check for IFL12H row profiling
Icon Description
Main menu
  • System resistance (in the absence of an insulation fault)

  • Measurement parameters menu

  • Monitoring menu

  • System resistance as primary record in Logging page

Fault log menu
Setting parameters menu and submenu
Display language selection menu
Product identification
  • Indication of an insulation alarm

  • Indication of product status

  • Indication of channel status

Summary
No alarm
Alarm
Toroid disconnect
Date/Time parameters menu
Insulation alarm parameters menu
I/O configuration parameters menu
Modbus parameters menu
Commission parameters menu
Password parameters menu
Display parameters menu
Reset parameters menu

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?