7EN02-0407-04

Changing the channel name

  1. Navigate to Menu > Settings > Network > Channel Name.
    The CHANNEL NAME screen displays with the channel grid and a flashing dot on the channel 1 grid. This indicates the channel 1 is selected.
  2. Perform any one of the following:

    • To modify the name for channel 1, press button.

    • To modify the name for other channels, press button to navigate to the desired channel and press button.

    • To modify the name for all channels, press button and press button.

    The CHANNEL NAME screen displays with the default name CHANNEL – 1 and the character C highlighted.

  3. Press the button.

    The CHANNEL NAME screen displays and the default name is deleted and the screen is blank.

    • To delete the channel name, see Deleting the channel name.

    • To modify the channel name, press the button.

      The CHANNEL NAME screen displays and the highlighted character displays blank character.

      Use the button to navigate to the desired character.

      NOTE: On each press of button, the characters are looped in the following sequence:
      1. A to Z

      2. a to z

      3. 0 to 9

      4. Special characters (Minus (-),Slash (/), Percent(%), Full stop (.),(blank))

  4. Press the button and navigate to the next character.
  5. Perform to update the selected character.
  6. Perform and for other characters.
  7. Press the button to confirm the channel name.
    A Saved message displays.
  8. Press the Esc button.
    The CHANNEL NAME screen displays with the channel grid and a flashing dot on the channel 1 grid. This indicates the channel 1 is selected.
  9. Perform to to change other channel names.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?