7EN02-0407-04

China Standard Compliance

This product complies with the following standard(s) in China:

IEC 61557-9:2014 Electrical safety in low voltage distribution systems up to 1 000 V a.c. and 1 500 V d.c. - Equipment for testing, measuring or monitoring of protective measures - Part 9: Equipment for insulation fault location in IT systems

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.