7EN02-0421-03

Manual commissioning

The device must be manually commissioned if the connected toroid is not one of the recommended toroids.

NOTE: Refer to the Vigilohm catalog for the most up to date listing of compatible toroids.
  1. Navigate to Menu > Settings > Commissioning > Manual.
    The Manual screen displays with the channel grid and a flashing dot on the channel 1 grid. This indicates the channel 1 is selected.
  2. Perform any one of the following:

    • To commission channel 1, press button.

    • To commission other channels, press button to navigate to the desired channel and press button.

    • To commission all channels, press button and press button.

    The Toroid Turns screen displays.

  3. Set the toroid turns (Allowed values: 300 to 3000) and press the button. To set the toroid turns, see Parameter modification using the display.

    • If the turn ratio is valid, the Saved message displays.

    • If the turn ratio is not valid, the Error message displays. Select the correct turn ratio.

  4. Press Esc button.
    The Manual screen displays with the channel grid and a flashing dot on the channel 1 grid. This indicates the channel 1 is selected.
  5. Perform and for other non commissioned channels.
QR code for this page

Was this helpful?