IP Network Services
Description
This page allows you to configure the settings and activate the IP network services.
IP Network Services Configuration Procedure
Step |
Action |
Result |
---|---|---|
1. |
From the menu bar, click . |
Opens the menu. |
2. |
From the menu, in the submenu, click . |
Displays the IP Network Services configuration options. |
3. |
Enter HTTP/Web, HTTPS, Modbus TCP, ION Pass Through, Modbus TCP proxy (for slave mode), Discovery, DNS and SNMP port parameters. |
Selects the IP Network Services port options. |
4. |
Click . |
Updates the IP Network Services port settings of Link150 gateway. |
IP Network Services Parameters
Parameter |
Description |
Settings |
---|---|---|
|
Allows you to set the port number of the HTTP/Web server. |
1–65534 Default setting: 80 |
|
Allows you to enable or disable the HTTPS service and to set the port number of the HTTPS server. |
1–65534 Default setting: 443 |
|
Allows you to enable or disable the Modbus/TCP service. |
1–65534 Default setting: 502 |
|
Allows you to enable or disable the ION PassThrough service. |
Enabled Disabled (Factory Setting) |
|
Allows Modbus TCP master to get the data from slave of Link150 gateway. This is applicable only if Link150 gateway is in slave mode. |
Enabled Disabled (Factory Setting) |
|
Amount of time the Link150 will wait for a remote Modbus TCP/ IP device to respond to a Modbus TCP/IP connection request initiated by the Link150. This is applicable only if Link150 gateway is in slave mode. |
0.1–10 seconds Default: 3 seconds (Factory setting) |
|
Amount of time the Link150 will wait for a remote Modbus TCP/ IP device to respond to a Modbus TCP/IP request initiated by the Link150. This is applicable only if Link150 gateway is in slave mode. |
0.1–10 seconds Default: 2 seconds (Factory setting) |
|
Allows you to enable or disable the DPWS service. |
Enabled (Factory Setting) Disabled |
Allows you to enable and disable the silent mode and also to set the port number. |
1– 65534 Default setting: 5357 |
|
|
Allows you to set the port number of the DNS server. |
1– 65534 Default setting: 53 |
|
Allows you to enable or disable the SNMP service. |
Enabled Disabled (Factory Setting) |
Allows you to set the listening and notification ports. |
Listening Port:
Notification Port:
|