Special Features

Refer to 2110CT9701, 1640CT0801, 4620CT9601

Panelboard Special Features


  • Main circuit breaker without overload trip — Automatic Molded Case Switch (Not UL Listed)

  • Shunt Trip Circuit Breakers

  • Other Special Features — For information on the following special features, please see the Supplemental and Obsolescence Digest.

    • PowerLogic metering [1]

    • Customer equipment space (NQ and NF) [1]

    • Increased box depth [1]

    • Increased gutters–top, bottom, and sides [1]

    • Non-standard paint [1]

    • Welded base channel [1]

    • Type 1 gasketed [1]

    • Type 2 drip hood [1]

    • Type 3R/4/4X/5/12 stainless steel enclosure [1]

    • Type 4X fiberglass enclosure [1]

    • Stainless steel trim front [1][1]

    • Padlockable hasp [1]

    • Special locks (Corbin, Yale, Best) [1]

    • Equal height boxes [1]

    • Common trim to cover two equal height boxes [1]

    • Panelboard skirthides conduits feeding a panelboard [1]

    • Panelboard wirewayfor terminating conduit in wireway endwall [1]

    • Keyed mechanical interlocking of two or more circuit breakers (I-Line) [1]

    • Motor operators (I-Line only)

    • Panelboard interiors and special fronts to fit existing boxes

    • A standard panelboard box has one blank endwall and one with knockouts. Blank endwalls or knockouts in both endwalls are also available [1]

Footnotes

  1. Supported by the Panelboard Product Selector.
Feedback