Selection Procedure for NF Merchandised Panelboards

Refer to NF Panelboards

Selection Procedure for NF Merchandised Panelboards

  1. Review maximum electrical system voltage, ampacity, and available fault current, and determine the type of panelboard is desired (see NF Panelboards and I-Line Series Connected Circuit Breaker Ratings ).

  2. Identify total quantity of branch circuit breaker poles and panel spaces required (see Digest sections 7 and 9 for catalog numbers).

  3. Select proper main lug interior from NF Main Lug Interiors or:

    • Select main circuit breaker interior and main circuit breaker adapter kit from NF Main Circuit Breaker Interiors - 600Y/347 Vac Max. based upon the equivalent number of poles and ampere rating.

      note

      Interiors include solid neutral and are field convertible to top-feed.

    • If a main circuit breaker interior was selected, select a vertical main circuit breaker (or fuse) from PowerPacT H-, J-, L-, or LA/LH frame circuit breakers pages in Section 7 or a back-fed E-frame circuit breaker from Section 9 of the Digest.

  4. Select ground bars from tables NF Accessories and any non-standard neutral assembly
    (i.e., 200% neutral for non-linear loads) from NF Merchandised Neutrals.

    • Please note that an aluminum ground bar kit is included with NF Panelboard Interiors.

  5. Select any required sub-feed circuit breakers, sub-feed lugs (SFL), or feed-through lugs (FTL) kits:

    • Subfeed circuit breaker (SFB), sub-feed lugs (SFL) or feed-through lugs (FTL) kits: Modifications (Single- or Three-phase) in the NF Accessories sections.

    • For subfeed circuit breakers, select PowerPacT H-, J-, L- frame circuit breaker from Section 7 of the Digest.

  6. Determine the total enclosure height required by adding requirements from interior, main circuit breaker, neutrals, SFL, FTL, or sub-feed circuit breaker.

  7. Select enclosure from the tables NF Special Features Standard NEMA Type 1 Enclosure Selection Table—Enclosure Catalog Number for Standard Main Mechanical Lugs Only and Special Features Enclosures Selection Table—Merchandised NF Vertically Mounted Main Breaker Panelboards with Accessories (by Mains Rating).

    NEMA Type 1—select box and front (cover) catalog number corresponding to interior catalog number.
    NEMA Type 3R, 5, 12—select enclosure. Cover for Type 3R, 5, 12 is included with the enclosure.

  8. Select the branch circuit breakers to be installed in the panel.

    For NF panelboards, use E-frame circuit breakers from E-frame Thermal-magnetic (480Y/277 Vac Max) Maximum allowable branch breaker pair combination = 170 A.100 A Maximum at 600Y/347 Vac.

  9. Select options and accessories from tables NF Merchandised NeutralsAdd-On Lugs for Neutral Bars or Ground Bars.

    note

    Additional NF and NQ options may be found in the Supplemental Digest, Section 4.

NF Merchandised Selection Example
480Y/277 Vac, 3Ø4W, 25 kA SCCR, fully rated, copper bus, 100 A, main circuit breaker, Type 1, flush-mount, bolt-on, branch circuit breakers

Branches

Table No.

Catalog Number

Spaces

(13) 20/1

E-frame Thermal-magnetic

EGB14020 13
one 40/2

E-frame Thermal-magnetic

EGB24040 2
one 50/3

E-frame Thermal-magnetic

EGB34050 3
      Total 18 spaces
       
     

Min. Box Height

125 A MLO Cu Bus Interior

NF Main Lug Interiors

NF418L1C
With Main Circuit Breaker Adapter Kit

NF Main Circuit Breaker Interiors

N150MH 38 inches
Main Circuit Breaker Section 7 HGL36100
       
Enclosure (Box)

NF Main Circuit Breaker Interiors

MH38
Front (Cover)

NF Main Circuit Breaker Interiors

NC38F
      Total 38 inches
Feedback