NVE3860702-09

Meter screen navigation

The meter’s buttons and display screen allow you to navigate data and setup screens, and to configure the meter’s setup parameters.
  1. Press the button below the appropriate menu to view that screen

  2. Press the right arrow to view more screens

  3. In setup mode, a small right arrow indicates the selected option

  4. In setup mode, a small down arrow indicates that there are additional parameters to display. The down arrow disappears when there are no more parameters to display.

  5. In setup mode, press the button under Edit to change that setting. If the item is read-only, cannot be configured with the meter’s existing setup, or can only be configured using software, Edit disappears.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.