NVE3860702-09

PM2225C meter model

The meter is available in one model with optional accessories that provide various mounting options.

Meter models

Model Commercial reference Description
PM2225C

METSEPM2225C

Front panel mount, 96 x 96 mm form factor, EasyLogic VAF Power and Energy meter with RS-485 communication and digital I/O capabilities. Complies with accuracy class 1.

METSEPM2225CL05

Front panel mount, 96 x 96 mm form factor, EasyLogic VAF Power and Energy meter with RS-485 communication and digital I/O capabilities. Complies with accuracy class 0.5S.

METSEPM2225C2AI2AO

Front panel mount, 96 x 96 mm form factor, EasyLogic VAF Power and Energy meter with RS-485 communication and analogl I/O capabilities. Complies with accuracy class 0.5S.

METSEPM2225C2DI2RO

Front panel mount, 96 x 96 mm form factor, EasyLogic VAF Power and Energy meter with RS-485 communication and relay output capabilities. Complies with accuracy class 0.5S.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.