NVE3860702-09

Available standard alarms

Your meter has a set of standard alarms.
NOTE: Some alarms do not apply to all power system configurations. For example, line-to-neutral voltage alarms cannot be enabled on 3-phase delta systems. Some alarms use the system type and the VT or CT ratio to determine the maximum allowed setpoint.
Alarm label Valid range and resolution Units
ION Setup Display ION Setup Display
Over Phase Current Over Current, Ph 0.000 to 99999.000 0 to 99999 A
Under Phase Current Under Current, Ph 0.000 to 99999.000 0 to 99999 A
Over Voltage L-L Over Voltage, L-L 0.00 to 999999.00 0 to 999999 V
Under Voltage L-L Under Voltage, L-L 0.00 to 999999.00 0 to 9999999 V
Over Voltage L-N Over Voltage, L-N 0.00 to 999999.00 0 to 9999999 V
Under Voltage L-N Under Voltage L-N 0.00 to 999999.00 0 to 9999999 V
Over Active Power Over kW 0.0 to 9999999.0 0 to 9999999 kW
Over Reactive Power Over kVAR 0.0 to 9999999.0 0 to 9999999 kVAR
Over Apparent Power Over kVA 0.0 to 9999999.0 0 to 9999999 kVA
Leading True PF Lead PF, True -1.00 to -0.01 and 0.01 to 1.00
Lagging True PF Lag PF, True -1.00 to -0.01 and 0.01 to 1.00
Over Frequency Over Frequency 0.000 to 99.000 Hz
Under Frequency Under Frequency 0.000 to 99.000 Hz
Over Voltage THD Over Voltage THD 0.000 to 99 %

Over Present Active Power Demand

Over kW Dmd, Pres

0.0 to 9999999.0

0 to 9999999

kW

Over Last Active Power Demand

Over kW Dmd, Last

0.0 to 9999999.0

0 to 9999999

kW

Over Predicted Active Power Demand

Over kW Dmd, Pred

0.0 to 9999999.0

0 to 9999999

kW

Over Present Reactive Power Demand

Over kVAR Dmd, Pres

0.0 to 9999999.0

0 to 9999999

kVAR

Over Last Reactive Power Demand

Over kVAR Dmd, Last

0.0 to 9999999.0

0 to 9999999

kVAR

Over Predicted Reactive Power Demand

Over kVAR Dmd, Pred

0.0 to 9999999.0

0 to 9999999

kVAR

Over Present Apparent Power Demand

Over kVA Dmd, Pres

0.0 to 9999999.0

0 to 9999999

kVA

Over Last Apparent Power Demand

Over kVA Dmd, Last

0.0 to 9999999.0

0 to 9999999

kVA

Over Predicted Apparent Power Demand

Over kVA Dmd, Pred

0.0 to 9999999.0

0 to 9999999

kVA

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.