NVE3860702-09

Meter overview

The PM2225C meter is a digital meter that offers comprehensive 3-phase electrical instrumentation and load management facilities in a compact and rugged package.

The meters offer value for the demanding needs of your energy monitoring and cost management applications. All meters in the PM2225C range comply with Class 1 or Class 0.5S accuracy standards and feature high quality, reliability and affordability in a compact and easy to install format.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.