NVE3860702-09

Instantaneous

The meter provides highly accurate 1-second measurements, average values, including true RMS, per phase and total for:
  • Per phase and average voltage (line-to-line, line-to-neutral)

  • Per phase and average current, and neutral current

    NOTE: Neutral current is calculated.
  • Per phase and total power (VA, W, Var)

  • Per phase and average for true and displacement power factor

  • System frequency

  • Per phase and maximum of all three for voltage unbalance and current unbalance

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.