NVE3860702-09

Configuring the LED for alarms using ION Setup

You can use the ION Setup to configure your meter’s LED for alarming.
  1. Open ION Setup and connect to your meter. See the ION Setup Help for instructions.
  2. Navigate to Energy Pulsing.
  3. Select Front Panel LED and click Edit.
  4. Set the control mode to Alarm and click OK.
  5. Click Send to save your changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.