NVE3860702-09

Power quality

The meter provides complete harmonic distortion metering, recording, and real-time reporting, THD percentage for all voltage and current inputs.

The following power quality measurements are available:

  • Total harmonic distortion (THD%) for current and voltage (displays line-to-line or line-to-neutral, based on selected system configuration)

  • Individual odd harmonics up to 15th order (Voltage and current, per phase)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.