NVE3860702-09

Setting up the screen passwords

It is recommended that you change the default password in order to prevent unauthorized personnel from accessing password-protected screens such as the diagnostics and reset screens.

This can only be configured through the front panel. The factory-default setting for all passwords is “0” (zero).

  1. Navigate to Maint > Setup.
  2. Enter the setup password (default is “0”), then press OK.
  3. Navigate to HMI > Pass.
  4. Move the cursor to point to the parameter you want to modify, then press Edit.
    Parameter

    Values

    Description

    Setup 0000 - 9999 Sets the password for accessing the meter setup screens (Maint > Setup).
    Energy Resets 0000 - 9999 Sets the password for resetting the meter’s accumulated energy values.
    Demand Resets 0000 - 9999 Sets the password for resetting the meter’s recorded peak demand values.
    Min/Max Resets 0000 - 9999 Sets the password for resetting the meter’s recorded minimum and maximum values.
  5. Modify the parameter as required, then press OK.
  6. Move the cursor to point to the next parameter you want to modify, press Edit, make your changes, then press OK.
  7. Press the up arrow to exit.
  8. Press Yes to save your changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.