NVE3860702-09

Setting up regional settings

You can change the regional settings to localize the meter screens and display data in a different language, using local standards and conventions.
NOTE: In order to display a different language other than those listed in the Language setup parameter, you need to download the appropriate language file to the meter using the firmware upgrade process.
  1. Navigate to Maint > Setup.
  2. Enter the setup password (default is “0”), then press OK.
  3. Navigate to HMI > Region.
  4. Move the cursor to point to the parameter you want to modify, then press Edit.
  5. Modify the parameter as required, then press OK.
  6. Move the cursor to point to the next parameter you want to modify, press Edit, make your changes, then press OK.
  7. Press the up arrow to exit.
  8. Press Yes to save your changes.

    Regional settings available using the display

    Parameter

    Values

    Description

    Language English US, French, Spanish, German, Portuguese, Chinese, Russian and Turkish Select the language you want the meter to display.
    Date Format MM/DD/YY, YY/MM/DD, DD/MM/YY Set how you want the date to be displayed, e.g., month/day/year.
    Time Format 24Hr, AM/PM Set how you want the time to be displayed, e.g., 17:00:00 or 5:00:00 PM.
    HMI Mode IEC, IEEE Select the standards convention used to display menu names or meter data.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.