NVE3860702-09

Panel meter

The back of your meter supports various power system connections.
A Auxiliary power supply (control power) terminals (L+, L-)
B Input voltage terminals (V1, V2, V3, VN)
C I/O card
D RS-485 communications (D0, D1, SHLD, 0V)
E Gasket
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.