NVE3860702-09

Feature summary

Parameter PM2225C
Accuracy Class for Wh

Class 1 or Class 0.5S

Accuracy Class for VARh

1.0

Sampling rate per cycle 64
Current:
  • Per-phase and 3 phase average

  • Calculated neutral current

ü
Voltage:
  • V L-N - per-phase and 3 phase average

  • V L-L - per-phase and 3 phase average

ü
Power Factor
  • Per phase and 3 phase total

True PF

Displacement PF

Frequency ü
Power:
  • Active power (kW) - Phase wise and total

  • Apparent power (kVA) - Phase wise and total

  • Reactive power (kVAR) - Phase wise and total

ü
3 Phase unbalance

Current

Voltage

Demand parameters (kW, kVA, kVAR, I)

  • Last demand

  • Present demand

  • Predictive demand

  • Peak demand: Timestamp for peak demand *

ü

Energy: kWh, kVAh, kVARh (4 Quadrant) - Phase wise * and total

  • Delivered (Import / Forward)

  • Received (Export / Reverse)

Delivered (D)

Received (R)

Total (D+R)

Net (D-R)

Last cleared (Old) *

THD, thd:
  • Voltage L-N per phase

  • Voltage L-L per phase

  • Current per phase

ü

Individual Harmonics

Up to 15th individual harmonics

Min / Max with timestamp
  • V L-L average

  • V L-N average

  • Current average

  • Neutral current

  • Frequency

  • Active power, Total

  • Apparent power, Total

  • Reactive power, Total

  • Power factor, Total

ü
Communication RS-485 Modbus RTU

Digital IO modules (2 inputs & 2 outputs)

METSEPM2225C and METSEPM2225CL05

Analog IO Modules (2 inputs & 2 outputs)

METSEPM2225C2AI2AO

Relay IO Modules (2 digital inputs and 2 relay outputs)

METSEPM2225C2DI2RO

Retrofit

For configuring legacy communication data models

ü
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.