NVE3860702-09

Power demand calculation methods

Power demand is calculated by dividing the energy accumulated during a specified period by the length of that period.

How the meter performs this calculation depends on the method and time parameters you select (for example, timed rolling block demand with a 15-minute interval and 5-minute subinterval).

To be compatible with electric utility billing practices, the meter provides the following types of power demand calculations:

  • Block interval demand

  • Synchronized demand

  • Thermal demand

You can configure the power demand calculation method from the display or software.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.