NVE3860702-09

Input / Output

This section supplements the input and output installation and provides additional information regarding physical characteristics and capabilities

The input and output are available in the following variants:

  • PM2225C two channel analog input and output

  • PM2225C two channel digital input and output

  • PM2225C two channel digital input and relay output

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.