NVE3860702-09

Alarm priorities

Each alarm has a priority level that you can use to distinguish between events that require immediate action and those that do not require action.
Alarm priority Alarm display notification and recording method
Alarm LED Alarm icon Alarm details Alarm logging
High Blinks while the alarm is active. Blinks while the alarm is active. Alarm icon remains displayed until acknowledged. Click Details to display what caused the alarm to pickup or drop off. Click Ack to acknowledge the alarm. Recorded in alarm log.
Medium Blinks while the alarm is active. Blinks while the alarm is active. Click Details to display what caused the alarm to pickup or drop off. Recorded in alarm log.
Low Blinks while the alarm is active. Blinks while the alarm is active. Click Details to display what caused the alarm to pickup or drop off. Recorded in alarm log.
None No activity None None Recorded in event log only.
NOTE: The alarm LED notification only occurs if the alarm / energy pulsing LED is configured for alarming.

Multiple alarm considerations

If multiple alarms with different priorities are active at the same time, the display shows the alarms in the order they occurred.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.