BRU2456000_01

About the device

The Next Generation Saturn and Saturn Zen wall plates are a completely new electronic hardware and firmware implementation inside the existing Saturn and Saturn Zen (508xNL and R504xNL) designs.

The new versions include full color RGB indicators, temperature and humidity sensor, and upgradable firmware.

The new firmware supports existing features of Saturn and Saturn Zen wall plates, such as switching, dimming, timers, scenes, and corridor linking.

In addition, the new firmware has the following new/enhanced capabilities:

  • 4 Lighting Applications

  • 4 profiles

  • Per-key setting of ramp rate

  • Per-key setting of indicator on and off state color

  • 2 user-definable indicator colors

  • 5 dynamically controllable indicator colors

  • Enhanced scene capability

    • Multiple Lighting Applications

    • Per-element ramp rates

    • Scene Toggle/Ramp

  • Temperature and Humidity measurements via Measurement Application

  • High/Low Temperature and Humidity alarms

  • Sequences

  • Widget linking

Learn Mode  is deprecated and will no longer be supported on any new C-Bus devices.

The Restore to Previous power recovery option is deprecated and will no longer supported on any new  bus-powered C-Bus input devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.